Slewing rings from igus help add lively component to three-metre owls

Later this year, a unique work of art will enrich the vibrant cultural landscape of the US city of Austin, Texas. The interactive sculpture "Kempelen's Owls" will feature two Texas great-horned owls, each standing three metres tall. Lubrication-free and maintenance-free slewing rings from igus provide a surprise for the visitors

Profile

  • What was needed: PRT slewing ring
  • Requirements: the slewing rings had to be wide enough for mechanical cables, components and lighting elements to passed through them. They also had to withstand high axial and dynamic loads, and be maintenance-free despite the weather.
  • Success for the customer: the PRT slewing ring bearings from igus are resistant to chemicals, vibration-dampening and have low moisture absorption. They are also very robust and can withstand heavy loads.
Owl with PRT slewing ring bearing A lubrication-free and maintenance-free slewing ring bearing ensures the reliable movement of the head even in the most diverse weather conditions. (Source: igus GmbH)

"The axial and dynamic ranges are more than enough for the weight of the owl head, but also give us assurance if the public decides to climb onto the owl or pull its head."

Dan Sternof Beyer, Founder and Creative Director, New American Public Art

Problem

The challenge was finding a slewing ring bearing that could meet all the requirements needed for this application. New American Public Art has used igus in past projects, and worked with the company’s United States team in Providence, R.I., to find the best slewing ring for the large owls. "For this bearing, we needed a very specific set of qualities," he said. It had to be very wide to allow for mechanical and lighting elements to pass through it. This bearing needed to support a large axial and dynamic range to pose no hazard to the public, and be as maintenance-free as possible despite various weather conditions. This demanding list of qualities ruled out 90% of bearings on the market."

Solution

The sliding surface of the igus slewing rings is made of the high-performance polymer iglidur J, which is characterised by good chemical resistance, vibration dampening and low moisture absorption. The ring has an axial static load of 27,000 newtons and an axial dynamic load of 7,000 newtons. Thanks to the large PRT outer diameter of 450 millimetres, the sculpture requires less supporting material. The large inner diameter (430 millimetres) allows us to pass through fibre-optic cables, which light up the owls’ eyes at night,’’ Sternof Beyer explained. "The axial and dynamic ranges are more than enough for the weight of the owl head, but also give us assurance if the public decides to climb onto the owl or pull its head."

Technical drawing of the owl with PRT slewing ring bearing
The two Kempelen's Owls will soon be part of the Austin Artspace. Visitors can use a hidden mechanism to turn the owl head. (Source: igus GmbH)



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH