Hot party nights: spring cable drums for a movable nightclub ceiling

Mecaoctet increases the reliability and aesthetics of a dynamic lighting system

bronze vector award
Winner of the bronze vector award 2024: French company Mecaoctet has created a movable ceiling for a nightclub in the Accor Arena in Paris. For the power supply, the designers rely on slip-ring-free spring cable drums from the igus e-spool series. The vector award jury was impressed by the technical solution for the breathtaking light show. 

Profile

  • What was needed:  Slip ringless spring cable drum e-spool
  • Requirements: The designers have to supply moving LED strips with fail-safe power over a distance of six metres.
  • Industry: Stage technology
  • Success for the customer: Reliability, aesthetics and no need for complex coils with rotating collectors.

Problem

The movable nightclub ceiling consists of a fragmented mirror measuring 16 x 15 metres, which is divided into 32 triangular elements, 16 of which are movable. Each of these triangles has two mirror surfaces, one at the top and one at the bottom, with the edge consisting of an SRU LED strip. In combination with spotlights, a breathtaking light show with monumental shapes in motion is created above the heads of the guests. The design challenge was to set the triangles in motion and supply the LED strips with power. 

Solution

The engineers rely on three motorised winches at each corner of the triangles. For the power supply, the experts rely on slip-ring-free spring cable drums from the igus e-spool series, which are fitted with hybrid cables and connected to the centres of gravity of the triangles. The stroke of the application is six metres. The speed is 0.5 metres per second. According to Mecaoctet, thanks to the igus solution, complex coils with rotating collectors, which would have been very expensive and unreliable, could be avoided. Compared to a slider system with cable loops, the solution is also more fail-safe and aesthetically pleasing.

"During our discussions, the igus sales representative drew our attention to the e-spool flex solution."
MECAoctet
Energy chains
Energy chains
Energy chains


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH