Lightweight and maintenance-free plain bearings in steering system of racing car prototype

iglidur® plain bearings in the steering system withstand the high stresses of racing

Profile

  • What was needed: iglidur ® plain bearing
  • Requirements: Lightweight components were needed that work particularly reliably and maintenance-free in racing and are economical at the same time
  • Industry: Automotive, racing
  • Success for the customer: iglidur® plain bearings with low friction properties are used at various points in the steering system, which reliably withstand off-axis forces and thrust pressure; the use of spacer discs further reduced the wear of the plain bearings
Steering rod