Customer application examples

More than 5,000 active customers worldwide reduce costs with wear-resistant components made from igus 3D printing materials.

Printed positioning bars in cartoning machine
One-piece screw in conveyor system
Product turners for the packaging and beverage industry
3D-printed gripper fingers made of laser sintering material iglidur i3 for handling perfume bottles
3D printed gears in the roof-mounted water cannon of an airport fire-extinguishing vehicle
The gears printed in 3D in the stepper motor help swivel the searchlight.
The blood sample is taken from the patient and placed in the device.
The microscope camera
The illusion of the floating object can be achieved with two linear movements and one rotation.
DIY race car simulator
Special mounting bracket made of igumid P190 using the filament extrusion process to attach the energy chain of the 3D printer to the rail guide
A device manufactured from iglidur I190 in 3D printing so that the rails rest at right angles on the profile saw's working surface.
3D printed sliders in rope-free lift
A bevel gear drive made of iglidur i3 keeps to a precise schedule in the dispensers for personally packaged medications.
Device to compensate for the Earth's rotation in order to allow long exposures for astrophotography.
3D printed finger joints in therapeutic use
Rocket module for measuring the movement and position of objects in space
The ball bearings made of iglidur i150 minimize steering inaccuracy on the 3D-printed "Chameleon" vehicle.
3D printed lead screw in a fully automatic coffee machine
3D printed components for rear wings
Split prototype plain bearing made of iglidur i3
Glide pad adapter clips for the transition between glide pad and glide bar
3D-printed mechanical clockwork made of iglidur i150 filament
3D printed replacement parts in a grand piano
3D printed gear in a tractor
3D printed bearing in a pram
Replacement gears made of iglidur i3 for an e-bike planetary gearbox
Vintage speedometer
3D printed pinions in a racing car
3D printing prototyping for electrical vehicles
3D printed reverse thread roller in a winding machine
Gas ring with 3D printed components
3D printed sliding plates in mowing machines
3D printed sprockets
3D printed gripper
Gripper Corona test station
3D printed bearings in a camera dolly
For me, it was a perfect example of how Industry 4.0 works. It took just three weeks to move from the task to the real-world solution to a highly customised design problem, and only two hours were on the computer.

Consulting

I look forward to answering your questions

International company for Electrical Engineering, I.E.E. (Non-port business)+201144146285Write e-mail

Shipping and consultation