Pivoting and rotating: plain bearings for moving slats on an exterior facade

7300 iglidur® G bearings were installed at the service centre of an automobile manufacturer.

Profile

  • What was needed: iglidur ® G plain bearing
  • Requirements: In the steel-glass façade for a service centre of an automobile manufacturer, a partial opening of the façade was to be implemented with bearings. These must have a long service life, be maintenance-free, dirt-resistant and corrosion-resistant.
  • Sector: Façade technology
  • Success for the customer: Since the installation, the iglidur® bearings have ensured the trouble-free, safe and reliable movement of the exterior façade.
Glass louvre system from Fenster Keller GmbH