Successfully used in film and camera technology

Smooth-running energy chains for Tagesschau studio camera robots

Three camera robots are suspended under the ceiling of the Tagesschau studio to achieve smooth, highly precise camera movements. Smooth running, low vibration, and wear resistance are the main requirements for the energy chains for guiding the extensive cable packages. E6 chains and chainflex control cables are used.
More about the application
Cameras at the Tagesschau studio
e-chain at the Tagesschau studio

Robust energy chains for high-speed camera carriages

The Trackrunner from Rail & Tracking Systems is a professional fast-moving camera carriage used in sports competitions and TV shows. For the safe guidance of the cables, the company relies on energy chains of the E6 series, which easily master the high accelerations even outdoors at high temperatures.
More about the application
Camera carriage from Rail & Tracking Systems
Camera carriage from Rail & Tracking Systems

Compact rotary table bearing for 360° product shots

A solution that was as light and compact as possible and required only a few components was sought for the bearing and drive of the rotary disc. A high mechanical resilience combined with low speeds was also required. The choice fell on light and vibration-dampening iglidur PRT slewing ring bearings.
More about the application
Camera rotary table with PRT slewing ring
Camera rotary table with PRT slewing ring

Precise panning of a microscope camera with 3D printed clamps

Special clamps made from the slide-optimised iglidur i151 3D printing filament ensure that the motorised microscope camera system moves steadily and precisely in the ultra-precise deposition printer of the company XTPL.
More about the application
3D printed clamps for microscope camera
3D printed clamps for microscope camera

Precise and strong gearboxes from the 3D printer for rotating devices for astrophotography

In order to be able to take astronomical photos, the earth's rotation must be compensated for. This is made possible by a special device from vhw Digitalart, which can rotate exactly 360 degrees in 24 hours. The gears and mounts for the motor and electronics were made from the tribofilament iglidur i150 using 3D printing.
More about the application
Gearbox for astrophotography device
Camera rotary table with PRT slewing ring

Smooth running on the camera slider even with offset load

In Glidetrack's camera slider, the bearings were unevenly loaded when cameras were installed, whose centre of gravity was far outside the bearing axis. The result: tilting of the bearings and loud rattling. The solution: drylin WJRM hybrid bearings, which ensure significantly better operation. In addition, vertical and horizontal movements overhead are now also possible.
Camera slider from Glidetrack
Camera slider from Glidetrack

Precise, smooth focus adjustment of the large format camera

The Gibellini company was looking for a suitable linear guide to adjust the focus of their professional large format cameras. The choice fell on the lubrication-free drylin W system, which enables focusing with millimetre precision without the use of gear racks. The customer appreciates the jerk-free, fluid gliding movement.
Gibellini large format camera
Gibellini large format camera

Stable crane movements with maintenance-free plain bearings

In the EZFX jib, iglidur G plain bearings replace the previously used bronze bushings. They are lighter, more cost-effective and, thanks to their dry operation, do not require any additional lubrication, so there is no longer any need for maintenance.
iglidur G plain bearings in the camera crane
iglidur G plain bearings

Industrial USB cables for digital image processing

Due to their clean signal transmission and robustness, the camera manufacturer IDS recommends its customers our chainflex USB cables, which can be used up to a length of 10 metres.
More about the application
CFBUS cable to USB interface from IDS
CFBUS cable to USB interface from IDS


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH